STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! [Please ignore] STM32U5, ThreadX and CMSIS

[EDIT: S'OK, I need to think about this more, but I can't find a way to delete a message so am just marking this as one to ignore]I am just moving from STM32F4 to STM32U5.  ThreadX seems to be the thing for STM32U5 (if one doesn't want to use Zephyr)...

Problem with SD Card with STM32H743ZIT6

Hello, i am trying to make a file with a text on a SD card without success.I followed this tutorial:https://community.st.com/t5/stm32-mcus/how-to-create-a-file-system-on-a-sd-card-using-stm32cubeide/ta-p/49830But i have a stm32h743zit6 and it is a bi...

rubenles_0-1705580530944.png

Resolved! hal_stm32 on Zephyr 3.2.0

Hi everyone. I'm currently working on a legacy project that only runs on Zephyr V3.2.0. I have to use the hal_stm32 to get some peripherals running (https://github.com/zephyrproject-rtos/hal_stm32). The latest version of hal_stm32 is not compatible w...

RTC or timer?

Hello everyone,In my project on STM32 Nucleo-64 with STM32F401RE MCU, I use a timer (TIM11) at 32 Hz in interrupt mode to get some data from sensors.  Can I use the RTC (Real-Time Clock) instead of TIM11 to get these data at the same frequency?If yes...

STM32F767ZI MQTT Issue

Hi all, I have issue with stm33f767zi and LWiP mqtt. I'm trying to send data over mqtt every 10ms. Data is 400 samples from 3 ADCs represented as cJSON. After sending a few packets Im getting hardfault on tcp_out(), but if I set interval to 100ms eve...

USB Type-C IC suggestion

Hi,I'm looking for some suggestions for the implementation of a self-powered and DRD (Dual Role Data) system provided with USB Type-C connector, but without PD support.I found two different solutions:1) Using a configuration channels protection IC (T...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.