STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

What is limiting the UDP Rx?

Hey folks. My question up there is probably a bit vague.I'll try to formulate it more precisely and what I've done so far.So first of all, I don't use RTOS.I have a few data mapping and sending functions in my main loop. Actually, I should also put M...

Yoschii97 by Associate III
  • 4749 Views
  • 7 replies
  • 0 kudos

Resolved! IAP Jump to application not working

I am using STM32Cube Version: 1.15.0 Build: 20695_20240315_1429 (UTC) and on an STM32F767ZGTx with FW_F7 V1.17.1I have a running and tested application for which I am now including FW Update from SDCard.I got two examples on which to base the new cod...

ADC not working at all - only output is "0"

Hello,I am trying to continuously read a voltage from a single channel by using the onboard ADC of the STM32L562ZET6 on a custom PCB. All the relevant analog voltages of the ADC have expected values, i.e. VREF+ =  3V, AVDD = 3V VREF- = 0V, AVSS = 0V....

MBEDTLS_SSL_OUT_CONTENT_LEN

Hi, I'm working with STM32CubeMX and on MBEDSSL defined MBEDTLS_SSL_OUT_CONTENT_LEN at 2048.When I generate the code I get (/CM7/MBEDTLS/App/mbedtls_config.h):#define MBEDTLS_SSL_OUT_CONTENT_LEN 16384 Is there a problem?Am I making a mistake?My envir...

lonejack_0-1708501317704.png
lonejack by Associate III
  • 1773 Views
  • 1 replies
  • 0 kudos

Azure NetXDuo WebServer

Hi people,I'm using a STM32H7 with a NetXduo web server example. I implementend a http get endpoint to get some data and a http put endpoint to reset the mcu. Sometimes, after the reset, the network stops to work. The http get, put and even the ping ...

fernandes by Associate II
  • 3563 Views
  • 6 replies
  • 0 kudos

uds protocol

I'm student working on my end-of-studies project so I have to communicate with the cluster (display of cars) so when I read the documentation I find that I have to communicate CAN with them sending frame with my stm32 board but also I need to send so...

sana1_3-1714046162403.jpeg
sana1 by Associate III
  • 2301 Views
  • 2 replies
  • 1 kudos

stm32g431 works only after a restart

Hello STM community,I'm encountering a rather peculiar issue in my project. I'm attempting to send and receive data from a Simulink model using the Simulink Desktop Real-Time packet input-output blocks. I'm employing UDP communication with the W5500 ...

SELMA by Associate
  • 2627 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.