STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ADXL345 library development for STM32F407VG-DISC

Hi everyone, I am kinda new at Embedded programming and I wanna ask a question.I am working on a library development of ADXL345 sensor and when I read the datasheet of this sensor here is the information that I got:"An alternate I2C address of 0x53 (...

testbenchmark_0-1715498328928.png

X-Cube-STL

Bonjour,M-Extend est une société basée à Acigné près de Rennes en Bretagne. Nous sommes équipementiers agricoles et nous fabriquons essentiellement des chargeurs frontaux pour les tracteurs. https://m-x.eu/Je travaille au pôle innovation en tant qu'i...

STM32F765VIT6 and ADS131E08 code

Hello All, I hope you are all doing well !I m writing to ask help, I have problem with my STM32f765vit6 and an  ADS131e08 .My the ADS131E08 stops communicating over SPI in continuous mode after a few seconds and block the SPI communication again. But...

Azer by Associate
  • 2252 Views
  • 2 replies
  • 0 kudos

Resolved! f_write fails the 2nd time its called

Board: STM32F411REGreetings,I am trying to make a program where the mcu read an audio file on the SD card, apply a sound filter on it, and write the output to a different file. The program will split the audio file into small chunks and compute them ...

Resolved! stm32h743 library file for proteus

i need to add the stm32h743 in to the proteus , bcz i dont have the hardware.can anybody tell how to download stm32h743 library file for proteus  or  direct link to download file . thanks.....

OctoSPI configuration for hyperflash

does anyone have a configuration for the CypressS26KL256S hyperflash? in the stm32cube_fw_l4_v1130 are examples only for regular command mode (micron or macronix) but not for hyperflash mode. thanks in advance

Leo_Panda by Associate III
  • 7517 Views
  • 12 replies
  • 1 kudos

Stuck in application startup code

I am facing an issue on one of our stm32f4 boards. We have a custom bootloader , which boots up the app as below   __disable_irq(); HAL_RCC_DeInit(); __HAL_RCC_AHB1_FORCE_RESET(); __HAL_RCC_AHB1_RELEASE_RESET(); __HAL_RCC_AHB2_FORCE_RESET(); __HAL_...

krishr by Associate III
  • 2919 Views
  • 5 replies
  • 0 kudos

Resolved! building cloned project

Hi Team,I've recently cloned https://github.com/STMicroelectronics/STM32CubeL5/tree/master/Projects/STM32L562E-DK/Applications/USB-PD/USB-PD_Consumer_1port , for USB PD project.But when i imported the folder into workspace ,the build option is disabl...

NITHIN by Associate III
  • 4976 Views
  • 8 replies
  • 5 kudos

Resolved! when I build the project, it is showing the error of 1. .text' will not fit in region `FLASH' 2. `FLASH' overflowed by 12480 bytes

Hello everyone,I am working with stm32f070c6 , I am developing an application of USB_CDC , When I build the project it is showing the error of 1. .text' will not fit in region `FLASH'2. `FLASH' overflowed by 12480 bytesactually I had increase the hea...

RKUMA.2 by Associate II
  • 9178 Views
  • 6 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.