STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Identifying stm32F407 vs stm32F411

Is there any way at all in PC software (Either the ST libraries or things like libUSB) to identify whether a device in DFU/Bootloader mode is an F407 or F411? Everything I can find in the USB properties is identical between the two (Same VID/PID, sam...

FreeRTOS + LWIP + UDP

I'm trying to achieve a UDP communication with STM32H753IIT6 and LAN8720A.I use STM32CubeIDE 1.14.0.According to the ST Ethernet and LwIP  example:   Adam BERLINGER edited on ‎2023-12-07 , I create a project, and change the pin layout according to my...

Hamaos_0-1718185156794.png Hamaos_1-1718185655716.png Hamaos_0-1718186299828.png
Hamaos by Associate
  • 2913 Views
  • 1 replies
  • 0 kudos

x-cube-tcpp in real project

We plan to use STM32G0 mcu with UCPD interface and external TCPP03-M20 protection circuit with single bi-directional power path in our smart power bank with replaceable smart battery and USB-C PD dual role power port application. There will be one US...

Resolved! HAL_SAI_Transmit_IT data

I'm using the NUCLEO board NUH723 to develop a project and I need to understand better how the HAL_SAI_Transmit_IT works. In my code I use the HAL_SAI_Transmit_IT to send data to the SAI1 interface --> 48KHz, stereo,32bit: I have to send two buffer o...

carloV by Associate III
  • 1753 Views
  • 1 replies
  • 0 kudos

Interupting CAN communication

Hello everyone. I am working on CAN communication with STM32F429I-Disc1 with TJA1050 transceiver. Standard communication works more than fine. What I would like to do next is to interrupt communication while CAN message with certain ID is present on ...

kingston by Associate
  • 2275 Views
  • 3 replies
  • 0 kudos

Resolved! ST-WDS software [fixed]

The ST MIcro website offers this free tool link but when I download it, its appears to be resticted as a trial use.I followed the instructions and there was a link on the download page that gets installed, simple and good for a year.Thanks 

Include a bin file to my project

Hello to alli have build my project as programmer on stm32f103c8t6 to connect as master host to slave one stm32f103c8t6 and program the slave device with code which saved in eeprom connected to the master with i2c it working well with me but I need t...

Elmofty by Associate II
  • 4043 Views
  • 5 replies
  • 1 kudos

Resolved! SPI MISO shifted

Hello ST Community, I have setup a SPI master and a SPI slave, both use DMA in Normal mode. The word size is 8-bits and the data size is 8-bytes. The problem is that the slave transmits messages which contains old data. When it should send:MISO: { 0x...

Nikolaj_TL_0-1718698066796.png {02530675-2C30-4D84-BCB1-AEE662778433}.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.