STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! GPIO Interrupt

Is it possible to disable a specific GPIO interrupt in my code and re-enable it after some time. HAL_NVIC_DisableIRQ(EXTI4_15_IRQn) this function will help but this will disable all the GPIO pins connected to that particular EXTI line. Any other poss...

STM32U545 Nucleo Fails to Initialize SDMMC

Hello, I am attempting to use an STM32U545 nucleo board with an external SD card shield from Adafruithttps://www.adafruit.com/product/4682However, each time I attempt to initialize the SDMMC peripheral, the call to HAL_SD_Init fails with a DTIMEOUT e...

aroby95 by Associate II
  • 1578 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H743 USB code generation problem

I'm using an embedded hardware design based on the NUCLEO-H743ZI. Within the SMT32CubeIDE I configured all of the pins and set up the clock according to my PCB, I'm using an external LSE 32.768Khz and no external HSE. The PCB is set up to utilize VBU...

Erric by Associate
  • 1655 Views
  • 1 replies
  • 0 kudos

Resolved! lwip cgi help

Can anyone help me please?I'm using LWIP and CGI SSI and http webserver. I've written an html form on my webserver that when submitted sends 16 parameters (each of 32 byte length) as a get. This crashes my webpage and the code never reaches the cgi h...

###### by Senior II
  • 6233 Views
  • 6 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.