2024-08-13 2:43 PM
Hello,
I am attempting to use an STM32U545 nucleo board with an external SD card shield from Adafruit
https://www.adafruit.com/product/4682
However, each time I attempt to initialize the SDMMC peripheral, the call to HAL_SD_Init fails with a DTIMEOUT error. I have tried mirroring the settings used in the STM32U5-Eval example included with the cube, however this too fails. Below are the settings being used to initialize the peripheral, generated directly from the Cube.
void MX_SDMMC1_SD_Init(void)
{
/* USER CODE BEGIN SDMMC1_Init 0 */
if (HAL_GPIO_ReadPin(GPIOC, GPIO_PIN_3) != GPIO_PIN_SET) return;
/* USER CODE END SDMMC1_Init 0 */
/* USER CODE BEGIN SDMMC1_Init 1 */
/* USER CODE END SDMMC1_Init 1 */
hsd1.Instance = SDMMC1;
hsd1.Init.ClockEdge = SDMMC_CLOCK_EDGE_FALLING;
hsd1.Init.ClockPowerSave = SDMMC_CLOCK_POWER_SAVE_DISABLE;
hsd1.Init.BusWide = SDMMC_BUS_WIDE_1B;
hsd1.Init.HardwareFlowControl = SDMMC_HARDWARE_FLOW_CONTROL_DISABLE;
hsd1.Init.ClockDiv = 1;
if (HAL_SD_Init(&hsd1) != HAL_OK)
{
Error_Handler();
}
/* USER CODE BEGIN SDMMC1_Init 2 */
/* USER CODE END SDMMC1_Init 2 */
}
void HAL_SD_MspInit(SD_HandleTypeDef* sdHandle)
{
GPIO_InitTypeDef GPIO_InitStruct = {0};
RCC_PeriphCLKInitTypeDef PeriphClkInit = {0};
if(sdHandle->Instance==SDMMC1)
{
/* USER CODE BEGIN SDMMC1_MspInit 0 */
/* USER CODE END SDMMC1_MspInit 0 */
/** Initializes the peripherals clock
*/
PeriphClkInit.PeriphClockSelection = RCC_PERIPHCLK_SDMMC|RCC_PERIPHCLK_CLK48;
PeriphClkInit.IclkClockSelection = RCC_CLK48CLKSOURCE_HSI48;
PeriphClkInit.SdmmcClockSelection = RCC_SDMMCCLKSOURCE_CLK48;
if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInit) != HAL_OK)
{
Error_Handler();
}
/* SDMMC1 clock enable */
__HAL_RCC_SDMMC1_CLK_ENABLE();
__HAL_RCC_GPIOC_CLK_ENABLE();
__HAL_RCC_GPIOD_CLK_ENABLE();
/**SDMMC1 GPIO Configuration
PC8 ------> SDMMC1_D0
PC12 ------> SDMMC1_CK
PD2 ------> SDMMC1_CMD
*/
GPIO_InitStruct.Pin = GPIO_PIN_8|GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_SDMMC1;
HAL_GPIO_Init(GPIOC, &GPIO_InitStruct);
GPIO_InitStruct.Pin = GPIO_PIN_2;
GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH;
GPIO_InitStruct.Alternate = GPIO_AF12_SDMMC1;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
/* SDMMC1 interrupt Init */
HAL_NVIC_SetPriority(SDMMC1_IRQn, 14, 0);
HAL_NVIC_EnableIRQ(SDMMC1_IRQn);
/* USER CODE BEGIN SDMMC1_MspInit 1 */
/* USER CODE END SDMMC1_MspInit 1 */
}
}
This issue happens regardless of if I use 1bit or 4bit mode on the SDMMC. A logic analyzer on the SDMMC lines showed no errors/issues, so at this point it feels like an issue in the HAL library. Debugging the code, I can see that values have been populated internally on the structures used by the HAL, but for whatever reason a DTIMEOUT occurs immediately after the first transaction from the peripheral and is never cleared, but is eventually checked by the HAL_SD_Init call which causes it to throw an error.
2024-08-14 11:31 AM
Hello @aroby95
This post has been escalated to the ST Online Support Team for additional assistance. We'll contact you directly.
Regards,
Roger
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.