STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! reset an stm32f746 discovery

Hi all, on stm32f746 disco, I'm using the Mbed ide but i have the stmcube installed as wellI've been writing a simple updater app that sits at 0x080e0000 with mixed success  switching to a previous project, the code downloads but on running the board...

andy0105 by Associate
  • 1440 Views
  • 1 replies
  • 1 kudos

STM32F427VGTx HAL_I2C_Mem_Write_DMA error

Hi, I have an issue using the HAL in question. I'm trying to write the following 4 characters 'C', 'i', 'a', 'o' to the EEPROM at address 0x0000, but what I observe through the analyzer is that the first character 'C' is being lost.Instead, the read ...

2024-09-13 12_41_11-Logic 2 [Logic - Connected] [Session 0].png

Resolved! Using HAL NAND

Good afternoon. I am configuring a NAND memory using FMC on the STM32H7. I am dealing with the following scenario: HCLK = 80 MHz (to match the example in AN4761) and a NAND memory SkyHigh Memory S34ML01G1 Following all the calculations specified in A...

Resolved! NUCLEO H755ZI-Q no signal on CAN TX line

Hello,I'm developing an application based on the above mentioned NUCLEO board and need a CAN connection to control the board. I've done some embedded development, but this is my first time using an STM board, so please forgive my lack of experience.I...

NUCLEO G491RE FOR PWM INVERTER

Hello,I want to generate 6 PWM signals for a 3-phase inverter, with 2 complementary PWM signals per leg, including dead-time. Is there an example or a starting point for this using the NUCLEO-G491RE?Thanks for any help.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.