STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

x-cube-freertos kernel update to 11.1.0

Hi Is there a plan to update the x-cube-freertos Kernel to 11.1.0? Github repo: STMicroelectronics/x-cube-freertos: X-CUBE-FREERTOS (FreeRTOS™ software expansion for STM32Cube) provides a full integration of the FreeRTOS™ kernel in the STM32Cube envi...

nobody by Associate II
  • 996 Views
  • 0 replies
  • 0 kudos

Looking for PVD example with STM32G0

hello!  i have a question about the power voltage detector in (external input analog voltage) i have a adjustable power supply connected on the pin (using a nucleo-G0B1RE) i was thinking that if i drop the voltage on the pin under the vref int voltag...

ABasi.2 by Senior
  • 1762 Views
  • 2 replies
  • 0 kudos

STM32L452 TouchGFX and SD Card

Hello,I am using a custom board with the STM32L452RET. On this board:SPI1 is connected to an IIS3DWB accelerometer,SPI2 is connected to a 240x280 TFT display with an ST7789 controller and TouchGFX,SPI3 is used with FatFs to access an SD card, followi...

fmaesso by Associate II
  • 1858 Views
  • 1 replies
  • 0 kudos

STM32F070CBT6 Emulate Eeprom Issue

When using this microcontroller for emulate eeprom process, i got some problems like freezing at start-up, when writing OLED, sprintf function can not write characters- writes silly words. I am not sure if the problem is about my emualte_eeprom proce...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.