STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! X-CUBE-RC-CALIB library

Currently, I am working on an STM32L432 microcontroller, emitting a 20 kHz sine wave. The code is relatively simple, although I am getting a slightly different frequency. I have been looking for solutions and found an embedded software package called...

CRC32 Calculation STM32L071CBT

Hi all,I know similar issues have been discussed before but I have not been able to find another post with the same issue. I am trying to use a CRC32 calculation to validate my flash memory, I am using KEIL IDE and the STM32L071CBT.This has been my c...

STM32F746 and External SDRAM Problem

  Hello,I want to use external SDRAM as the LTDC framebuffer with the STM32F746 microcontroller. I can write and read the desired data to/from the SDRAM without any issues. However, when I activate the LTDC, during the SDRAM initialization and config...

johnLocke by Associate II
  • 1936 Views
  • 3 replies
  • 0 kudos

Resolved! FATFS + RTOS + touchgfx

I have a working project that simply writes to a a file on an SD card (Using STM32H7B3I-DK, Not Using RTOS).When I add it to a touchgfx project, f_mount() and f_open() return NO_FILE_SYSTEM. This happens even after f_mkfs() returns FR_OK. I have the ...

Resolved! STM32H563 and SPI DMA Transfer issue

I'm having an issue when using the DMA with SPI.  I'm using the SPI for a 320x240 LCD and want the DMA to help with blocking while transferring large amounts of data with touchGFX.I'm able to paint the screen one color just using the SPI but when I t...

PFlor.2 by Senior II
  • 6773 Views
  • 12 replies
  • 5 kudos

Resolved! STM32H745BIT3 - FDCAN - emotas software stack

Hi:I now have a STM32cubeIDE project now successfully sending FDCAN messages to PCAN View running on my laptop. I'm now trying to add the emotas CANopen FD single line software stack to send CANopen messages. I can not get my program to build without...

KennyD by Associate
  • 1443 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.