STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Integrating MCUboot into a project

Split from old thread: https://community.st.com/t5/stm32-mcus-security/information-about-mcuboot-and-illustrative-examples/td-p/689154 Hello @Jocelyn RICARD ,I'm looking for guidance on integrating Mcuboot into my project. I am using a NUCLEO-U5A5ZJ-...

Ade J.2 by Associate II
  • 6263 Views
  • 6 replies
  • 1 kudos

Resolved! Button push not changing LED status

I am working with the NUCLEO-C031C6 board and tried to to make the user push button toggle the user LED but it stays stuck with no change to the buttonStatus variable, always high (1).I added the counter variable to see if it is continuously incremen...

HPate.12 by Associate II
  • 2178 Views
  • 4 replies
  • 0 kudos

Ux_Host-CDC_ACM : Enumeration failure

Dear All,I am testing the demo project for the NUCLEO-C071 to implement the USB HOST CDC_ACM (USBX). Below are some doubts that arose after the initial tests:After using the wizard to create the demo project 'Ux_Host-CDC_ACM', opening the .ioc file s...

LMore.2 by Associate III
  • 4920 Views
  • 13 replies
  • 0 kudos

initialize FATFS for SDMMC in M4

Hi team        What is the correct procedure to initialize FATFS for SDMMC in M4? Kindly provide the application note of the procedure. We need to run eMMC in M4 core    EVK used : STM32H745I-DISCO   References code:  STM32CubeH7/Projects/STM32H745I...

Ashwath by Associate
  • 1051 Views
  • 1 replies
  • 0 kudos

Resolved! STM32H7 FMC + ST7789 LCD

Hi,I am trying to interface Stm32h745 controller with a 240x320 TFT LCD over FMC. Interesting thing is, when I manually control lcd control and data pins(Set them as GPIO_OUTPUT_PP), Lcd works, but when I switched to FMC it does not. Tried lots of ti...

baycanakcay_0-1743510687213.png baycanakcay_1-1743510841119.png

Resolved! The maxium length of buffer for USB HID SetReport

Hi,I would like to know why when I sent the 202 bytes from pc to dev-board via USB HID, the buffer size would only get 32 byte each time, (byte[0]-byte[31])*several times until finished print out all 202 bytes?Couldn't it recieved whole 202 bytes the...

CYH by Associate II
  • 1867 Views
  • 3 replies
  • 0 kudos

Resolved! Controlling WS2812B LED Strip With STM32

Hello,I'm new to STM32 and trying to learn exciting stuff. I want to light a single LED from my WS2812B strip. For example I will choose 6th LED on my computer and 6th LED on strip will light up.But I'm not sure where to start. How can I access to si...

salvi.a by Associate II
  • 23003 Views
  • 8 replies
  • 5 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.