STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F105RC USB HID device

Posted on December 09, 2014 at 18:12HelloI was using a nucleo F103 like explain in the thread ''Nucleo-F103RB + USB''.Now I have the finish board. In the finish board i am using a STM32F105RC.SO i change the compiler from STM32F10X_MD to STM32F10X_C...

lemac by Associate III
  • 670 Views
  • 0 replies
  • 0 kudos

g

Posted on December 03, 2014 at 22:44g #hal_uart_error_pe-uart-parity

hossam by Associate II
  • 1672 Views
  • 3 replies
  • 0 kudos

STM32F411, STM32CubeMX, USB Device for CDC

Posted on November 26, 2014 at 08:09STM32F411RCTx, LQFP64When using STM32CubeMX Ver4.4 to generate USB Device only code for CDC class, initialization is fine but cannot connect to PC (host).The STM32CubeMX generated code also has same problem as MDK...

bardeen by Associate
  • 1665 Views
  • 2 replies
  • 0 kudos

stm32f207 usb only multiple of 64 bytes can be send

Posted on April 10, 2013 at 10:04change by stm32 usb device VCP example: my send function: uint16_t VCP_DataTx (uint8_t* Buf, uint32_t Len) {  uint8_t i;  for (i=0;i<64;i++)    //only multiple of 64 bytes can be send   {  APP_Rx_Buffer[APP_Rx_ptr_in...

easylwl by Associate II
  • 3483 Views
  • 7 replies
  • 0 kudos

USB HS Host Unconfigures Device

Posted on March 20, 2014 at 21:13Was hoping there might be a few folks here with more USB knowledge than me. I am trying to implement a HS USB HID-class device on a STM32F427 using a SMSC USB3300 external PHY IC. I have succesfully implemented a si...

jvavra by Associate III
  • 1602 Views
  • 3 replies
  • 0 kudos

Stm32f427 system memory bootloader

Posted on November 29, 2014 at 12:54 i have custom board with STM32F427VI and want to boot from usart3 via bootloader inside system memory. boot0 pin is low and boot1 pin is NC. i dont want to switch boot pins. because eventually these pi...

0690X00000602z0QAA.jpg

Complete USB OTG power solution design

Posted on November 28, 2014 at 10:03Hi, I have been working on a power design that integrates with the STM32F401 utilizing OTG.  I would like to support OTG both as a host and device.  In addition, I would like to detect dedicated charging ports and...

Use STM32CubeF4 or Standard Peripherals or DIY?

Posted on November 26, 2014 at 02:01I can see that STM32Cube is the new hotness, but...I am starting a new project with the STM32F405xx and FreeRTOS (ideally the current rev 8.1.2).  It seems that there are lots of layers added to peripheral access ...

mduffy by Associate II
  • 1001 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.