STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB cable detection

Posted on July 01, 2015 at 12:01 I use a custom STM32F407 board. I want to detect USB FS cable presence (no matter to pc or charger). Here is what I did. First, the VBUS pin is initialized in usb_bsp.c USB_OTG_BSP_Init function, I di...

stm32f217 usb mass storage

Posted on December 21, 2013 at 11:00Hello, Im using STM32F217 Mmicrocontroller for my project. Can anybody help me in writing the code for usb mass storage. I have STM32F2xx_StdPeriph Library.In that I dont find any driver related to Usb. #usb-m...

STM32F0: Using bootloader through USB-UART.

Posted on July 06, 2015 at 17:30Hello everyone. At my device I have to make an opputunity to load a firmware through UART interface. I know, that it's possible to do using just USB-UART converter. At the F1 series for this purpose I should set the B...

using stm32f40 with freeRTOS

Posted on July 05, 2015 at 21:37Hello,I would like your tips about how to find information about stm32f40.We plan to use it with several devices suce as: I2C STMPE1601 keyboard ,  MHDR2X14  CAM Interface, can bus, SPI OLED, and more. From start read...

ranran by Senior II
  • 1729 Views
  • 2 replies
  • 0 kudos

STM32F205 has bad bootloader from factory?

Posted on May 11, 2015 at 20:16Hello,We have been using STM32F205VB6 in production for several years. In a recent batch we purchased a high percentage of processors the boot loader doesn't work over USB properly. We have a jumper tied to BOOT0 pin a...

cmeyers by Associate II
  • 2786 Views
  • 8 replies
  • 0 kudos

STM32F103RBT6 and SD Card with FAT32

Posted on January 23, 2015 at 13:59 Hello. I have a project in which I want to log some data into a text file on a SD card, using STM32F103RBT6. I managed to program the interface driver through SPI, since this chip doesn't have SDIO. It works ...

HAL Library for Eeprom emulation

Posted on June 27, 2015 at 06:17Hi everybody, do we have any update on eeprom emulation library for HAL and CubeMX because the one in ST's site is still the old library for std_periph library ? #hal-eeprom-emulation

STM32CubeMX ETH PHY IRQ handler

Posted on June 11, 2015 at 13:20Hi, I was looking into how the generated code for an STM32F427 (with eth and lwip enabled) deals with ethernet status change events (network cable plug in/out, speed changes, ...). I could not find a polling loop, bu...

DMA IRQ handler can not call FreeRTOS API

Posted on June 26, 2015 at 04:01Hello,I am trying to add a semaphore within stm32_eval_i2c_ee.c IRQ handlers for synchronization. The current implementation polls a variable that is modified by the RX/TX IRQ handlers. Here is a link to a post on the...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.