STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L4 default DFU mode verus Standalone

Posted on August 05, 2015 at 17:25We used the DFUSE over USB successfully with several L152 designs. The L152 chips don t have a USB boot loader DFU like described in the AN2606 STM32 microcontroller system memory boot mode. (DFU SE via USB) So we d...

uwe2 by Associate II
  • 10714 Views
  • 29 replies
  • 0 kudos

Set a RTOS Uart queue with the HAL librarie

Posted on May 02, 2016 at 11:11Hi everyone, I would like to include in my project  FreeRTOS a uart queue. I have already  done this with the StdPeriph lib but I'm facing difficulties to migrate from StdPriph to HAL. My previous project was build l...

dauphin2 by Associate II
  • 2932 Views
  • 4 replies
  • 0 kudos

STM32F103VE USB Mass storage speed issue

Posted on April 27, 2016 at 10:55Hi,My application includes USB with mass storage class, I am using STM32F103VE MCU running at 72Mhz. Sandisk uSD(8GB, Class 10) used with SDIO  interface.I have used USB MSC code from STM32F1 library (STM32_USB-FS-De...

K_K by Associate III
  • 2295 Views
  • 5 replies
  • 0 kudos

STM32L0 USB CDC VCP Transmit problems

Posted on December 28, 2014 at 17:59I am using an STM32L053 part and trying to use the USB CDC VCP functionality on an STM32L0-Discovery board. In the past I've gotten the USB CDC VCP functionality working on an STM32F4 on a custom board using the S...

0690X00000605DyQAI.png
nlbutts by Associate II
  • 3303 Views
  • 6 replies
  • 0 kudos

STM32f429zit bootloader USB DFU problem

Posted on April 27, 2016 at 14:23Hello everyone,I have problem with my STM32F4 DISCOVERY board. According to spec:+ Using ''Bootloader (USB FS Device in DFU mode)''- Configure the STM32F4-Discovery board to boot from ''System Memory'' (boot pins BOO...

mateusz2 by Associate
  • 1673 Views
  • 2 replies
  • 0 kudos

DFU file not created

Posted on April 27, 2016 at 07:11Hi All:I am trying using DFU filemanager to generate the DFU files by V3.04 in Win 10.I followed my colleague's procedure and it showed file is created, however there is no any file is generated..Is any setting of pe...

jorgewu by Associate
  • 1171 Views
  • 1 replies
  • 0 kudos

DMA USB IN endpoint on STM32L476xx?

Posted on April 25, 2016 at 00:38Hello, I just read through the STM32L4x6 reference manual OTG chapter.  I understand that every received packet is multiplexed through 1 RX FIFO, but each outgoing endpoints have dedicated FIFO.  The RX multiplexing ...

hmc by Associate III
  • 861 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.