2016-04-18 2:02 AM
Hello,
I'm using the lwip stack in combination with FreeRTOS for a http server (Netconn API) and modbus TCP (FreeModbus). I'm using the lwip stack and FreeRTOS from the ''STM32Cube_FW_F7_V1.3.0''. Evriting works great for 10-20 min but after that time the processor crashes with a HardFault. The HardFault happens in the function tcp_output at the line ''if (TCP_SEQ_LT(ntohl(seg->tcphdr->seqno), ntohl(useg->tcphdr->seqno))) {''. The processor wants to load ''seg->tcphdr->seqno'' and ''useg->tcphdr->seqno'' but one pointer is not valid and the processor crashes at the address ''0800d50a'' with a HardFault and the flag unaligned memory access is set. I activated the lwip_stats and get 60 errors at the memp[6]. In the lwipopts.h the SYS_LIGHTWEIGHT_PROT ist set and I teset different configuration in the lwipopts.h but noting helped. Where can the problem come from? Here my disassembly: 1010 if (TCP_SEQ_LT(ntohl(seg->tcphdr->seqno), ntohl(useg->tcphdr->seqno))) { 0800d4fc: ldr r3, [r4, &sharp12] 0800d4fe: ldr r0, [r3, &sharp4] 0800d500: bl 0x80097d4 <lwip_ntohl> 0800d504: mov r6, r0 0800d506: ldr.w r3, [r8, &sharp12] 0800d50a: ldr r0, [r3, &sharp4] 0800d50c: bl 0x80097d4 <lwip_ntohl> 0800d510: subs r0, r6, r0 0800d512: cmp r0, &sharp0 0800d514: bge.n 0x800d546 <tcp_output+526> 1012 struct tcp_seg **cur_seg = &(pcb->unacked); #lwip #hardfault #stm32f7452016-04-18 2:18 AM
It looks like useg-tcphdr is not aligned. You could sanity check that it is 4-byte aligned, and memcpy out seqno, but this might just move the problem down stream.
2016-04-18 3:06 AM
I activated the MEMP_DEBUG and get the message:
memp_malloc: out of memory in pool TCP_PCB I increased the MEMP_NUM_TCP_PCB (for test purposes to 1000) but the meassage comes only later.2016-04-18 4:51 AM
A bit scary that it doesn't recognize calloc/malloc return NULLs
So perhaps you have a resource leak, or are getting heap fragmentation. The former you'd want to chase down by understanding who allocated the resource, and then that all exit/return paths handle the release properly. For the latter, a fixed size pool method, where different size allocations a pull from a size appropriate pools, so small but longer term allocations don't bisect large blocks of otherwise free memory.2016-08-15 8:54 PM
I am myo from sg. I am trying to run Modbus tcp server on stm32 f207zg.
do you have source code for your Modbus tcp project.
can you share with me.
my mail is
mailto:sayagyimyo@gmail.com
thanks in advance.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.