STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX I2S DMA buffer size

Posted on October 23, 2016 at 23:03Hi everybody, when using the Standard Peripheral Library I could set DMA buffer size for I2S using something like the following:   DMA_InitStructure.DMA_BufferSize = BUFFER_SIZE; But when using STM32CubeMX I could ...

fuentesj by Associate
  • 1087 Views
  • 0 replies
  • 0 kudos

Stm32F767 Nucleo Ethernet does not always start

Posted on September 18, 2016 at 03:00Hi All,I have noticed that the Stm32F767 Nucleo does not always start Ethernet reliably. For testing I used one of the example on the STM32Cube_FW_F7_V1.4.0 for the STM32F746ZG-Nucleo base of LWIP. I set up a DOS...

arainho by Associate II
  • 7704 Views
  • 20 replies
  • 0 kudos

Huawei 3G USB modem connect to STM32

Posted on August 15, 2016 at 19:37Hello. I try connect USB modem to STM32F207. I'm used AT^U2DIAG=0 command for switch modem to CDC mode. But in debug i see interfeise with bInterfaceClass = 0xFF only on modem. What is the interface? How get CDC?PC ...

zhenya by Associate
  • 1967 Views
  • 2 replies
  • 0 kudos

stm32 USB OTG Host doen't work with some usb-devices

Posted on September 06, 2013 at 09:20Hello. I am trying to use usb host in stm32f105. Done everything according to reference manual, usb libs, application notes, etc. The host works,but not always. To be more exact: not with all usb-devices. Keyboar...

maxim by Associate
  • 3855 Views
  • 7 replies
  • 0 kudos

STM32L4 USB Connect/Disconnect Detection

Posted on October 18, 2016 at 23:43I'm working on USB on an STM32L4 chip and cannot seem to reliably trigger when a USB Device is both Connected and Disconnected. I trigger the interrupt overall and handle it, but I need changes to happen as soon as...

jacob2 by Associate III
  • 3300 Views
  • 3 replies
  • 1 kudos

STM32L476VG USB CDC Not Recognized

Posted on October 12, 2016 at 19:56I'm working on a USB CDC project to get a virtual com port using an STM32L476VG processor, I have it configured to be a device only in hopes to simply pass information over the com port between my board and PC. I a...

jacob2 by Associate III
  • 2763 Views
  • 9 replies
  • 0 kudos

USB Virtual Com Port example

Posted on January 28, 2014 at 15:02Hello, USB Virtual Com Port example doesn't work on device modeI have a uC card wtih stm32f107 which works host and  FS mode, reads Flash disc.. Now I am trying eval vcp example, I made necessary changes but it doe...

arge by Associate III
  • 8767 Views
  • 10 replies
  • 0 kudos

Ethernet PHY Micrel 802RNLI Problem

Posted on October 17, 2016 at 20:20 Hello Guys, I have got a problem with the configuration of the ethernet PHY which I use. The problem occurs when i connect my PC and my custom board(which uses a STM32F107VCT). Under network settings I...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.