STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Partially configure GPIO using HAL

Posted on December 19, 2016 at 01:18Hello,I am trying to change pullup/down in GPIO. However, it looks like HAL_GPIO_Init() doesn't allow partial configuration of GPIO pin.Is there any way to configure pullup/down only using HAL? Should I change reg...

stm32f107 lwip freertos printf problem

Posted on December 19, 2016 at 16:05Hello;I am trying to implement FreeRTOS 9.0.0 and lwip2.0.0 with HAL library and GCCFor easiness I generated FreeRTOS code with STM32CubeMX and replaced FreeRTOS to 9.0.0 and then added LWIP. I can ping my device ...

Resolved! STM32F030C8 Interface with Quectel M95

Posted on December 07, 2016 at 12:59Hi all,I am working for a project which is having 5 interfacing modules out of this one module needs to interface quectel M95 GSM modem to stm32f030C8. From PCB side and Hardware all was done working fine modem Re...

I'm building a stm32f042 HID device/product, what are my options for updating it 'out in the wild'?

Posted on December 17, 2016 at 20:41The device uses the onboard USB capabilities of the stm32f042 and acts as a HID device.I trying to find the best way to update the device when it is out in the wild, what are my options for doing this?I would want...

USB HS in FS problem with CDC transmission

Posted on December 14, 2016 at 09:59H, I use STM32F439 in HS in FS mode with CDC class. Apparenty even though messages are received by uC  in proper fashion and sent to PC as I coded them,  terminals on PC fail to receive/display them right. If ther...

how to connect usb stick to Nucleo board

Posted on December 16, 2016 at 19:55Hi,I am using NucleoF401re board. I required to connect usb stick to the nucleo. i got following link with guidance. But i don't have LM3526 right now. So, is there any alternative to avoid LM3526 ic.?Or if i conn...

SS.Sagar by Associate III
  • 777 Views
  • 0 replies
  • 0 kudos

STM32 send USB packet bigger than 64B

Posted on December 16, 2016 at 18:16I'm currently developing on a Nucleo-144 (NUCLEO-F446ZE).When i want to send an answer to the pc with a packet bigger than maxpacket (64bytes)the HAL library split it witch is normal but it's not well receive by t...

thom_as by Associate II
  • 767 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.