STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB CDC Stuck in Transmit State STM32L4

Posted on May 23, 2017 at 21:00Little background knowledge, I'm trying to implement XMODEM protocol for a file transfer to my SD card and everything seems to be in place and working for the most part but I run into an issue occasionally on USBD_CDC_...

jacob2 by Associate III
  • 940 Views
  • 0 replies
  • 0 kudos

STM32F4 USB SERIAL

Posted on May 16, 2017 at 13:08Working on STM32F4 Discovery and using CubeMx to generate basic structure for the program.I am connecting FT232 based USB TTL Module to the USB OTG port of Discovery using Micro USB to Female OTG Cable.I am using CDC e...

anuj by Associate II
  • 2329 Views
  • 4 replies
  • 0 kudos

STM32F072 PowerOn Not in Run Mode

Posted on May 21, 2017 at 15:59I have STM32F072 Discovery board, I am running some demo program, now the issue is, when I power on the discovery with USB or external supply, it doesn't boot into run mode/Program Mode, I have to reset the MCU, in ord...

anuj by Associate II
  • 971 Views
  • 1 replies
  • 0 kudos

USB Device Description Request Failure Issue..

Posted on May 16, 2017 at 22:06Hi,I've a custom L476 board (battery powered,MSI 48MHz system clock, no HSE, no PLL) to implement USB MSC (OTG-FS). I'm using L4 Nucleo ST link extender to upload code on my Custom board. I've noticed that, when the cu...

0690X00000603TNQAY.jpg
rumlyen by Associate II
  • 1088 Views
  • 1 replies
  • 0 kudos

FatFS initialization on F072

Posted on May 13, 2017 at 16:26 Hello, I'm trying to port CubeMX repository example for uSD card on STM32F072-EVAL to NUCLEO-F For some reason I get error out of functionf_mount(...) which returns 11 (The logical drive number is invalid). Als...

serdes on STM32

Posted on May 18, 2017 at 18:52Are there any plans for an STM32 family product that implements a common SERDES interface for high speed communication with other chips (ie, FPGAs)?  Along with this, a PCIe endpoint in an STM32 would be much appreciat...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.