2016-01-25 9:35 AM
Hello
I observe
here
a strange phenomenon
,maybe
someone can help me
.
After a reset with boot 0 signal = high, the DFU mode does not start always. After the reset, it takes sometimes several 10 seconds until the DFU Mode starts. Sometimes I have to send a second reset. Was tested with a STM32F4 discovery and with our own board. On our board a STM32F405VGT6 1 is installed. On the Discovery a STM32F407VGT6 1. Both have the bootloader version 0x31. The Pins PA10, PB5, PB11 and PC11 are at a fixed level (GND or VDD) There seems to be a Race Condition to be, because it sometimes works 20 times in succession and then every other time not.It happens
regardless of whether
the
reset
is generated
by hardware
or
bootloader
via
NVIC_SystemReset()is called.
Has anyone ever seen this effect? And someone knows a solution for this? #stm32f4-dfu-usb-bootloader2016-01-25 10:15 AM
Perhaps there is a clock start issue, the System Loader benchmarks the HSE against a list of expected/supported frequencies using HSI.
2016-01-25 11:05 AM
That's what I
had thought too
.But
on the
Discovery
is an
8
MHz
clock
,which continues
even
after a reset
.On our
board
, it isa
16
MHz
clock
. But even there, it works sometimes.On our
board
the
clock
, however,is switched off
at reset
.The clock generator
starts
in
about 600
us to
a valid signal
.I have
further tested
with the
F4
Discovery
.When
R68
removed
and works with the
built-in
quartz
,then
again, the
clock
is stopped
after a reset
.Appears
the problem
(no
DFU
USB
Device
detected
),then
the
clock
remains stopped
until
the
DFU
mode is
recognized by the PC
.You can
reproduce
the effect by
GND
on
one puts
the
F4
Discovery
pins
PA10
,PB5
,PB11
and
PC11
(
I usehere
jumper
cable
)and
a
jumper
in
boot0
to VDD
sets
.If you press
the reset button
a few times
now
,then
the
DFU
USB
device
is not detected
on your PC
.
2017-05-19 3:00 AM
Hi Rolf,
Did you manage to find a solution for your problem? I think I'm having the same issue (see thread
), and still trying to find a workaround. Or, did you have to make a change to the board?We’re moving the ST Community to a new platform to give you a better and more reliable community experience.