STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB virtual com device(STM32F765ZI Nucleo)

Posted on September 14, 2017 at 18:45Hai., I am using STM32F767ZI NUCLEO board(144 pin), In this I need to use Full speed USB as Virtual com port device, I generated code using http://www.st.com/content/st_com/en/products/embedded-software/mcus-embe...

Nucleo F767ZI lwip and Hal interaction

Posted on September 16, 2017 at 00:24Greetings , I'm figuring out LWIP and the Ethernet setup on the above mentioned board. I've found the LWIP application note very useful in understanding LWIP and  Cube MX does extremely well to explain how to set...

Bug: STM32F0xx HAL SPI Transmit

Posted on September 23, 2016 at 11:35 I have found a bug in the STM32F0xx HAL SPI driver, specifically in the HAL_SPI_Transmit andHAL_SPI_TransmitReceive functions. Basically they are converting a pointer to uint8_t into a pointer to uint16_t. The...

UART Over-Run interrupt occurred in STM32F4

Posted on September 07, 2016 at 11:40Hi.....!!!I am using STM32F438IIT6 for UART Receive in Interrupt mode.I have used STM32Cube Mx for UART configuration & code generation.In Cube I have configured USART1 as followsMode: Asynchronous mode. H/W Flow...

sathya by Associate
  • 2437 Views
  • 4 replies
  • 0 kudos

Resolved! FatFS f_write does not work

Posted on September 09, 2017 at 00:21 Function f_write doesn't work correctly to write on SD card. Actually it calls a series of other function and one of them is HAL_SD_WriteBlocks which puts the mcu into Default_Handler: Infinite_Loop: ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.