STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F4 Discovery fatfs in ram windows 8

Posted on October 26, 2017 at 07:45I implemented mass storage in STM32F4 Discovery. Mass storage located in RAM it uses 64KB. I need just 16KB to load image from PC and draw it on LCD. Inside MCU I use ugfx and fatfs. It's almost working under windo...

urasinov by Associate II
  • 918 Views
  • 0 replies
  • 0 kudos

Resolved! F446RE System Memory Boot Mode UART1 PA9 Problem

Posted on October 24, 2017 at 10:38Hi, everyone. I got a strange, also interesting, problem, while I am using System Memory Boot Mode with STM32F446RE.=================================================================================Hardware Descript...

0690X00000608fpQAA.png 0690X00000608iPQAQ.png
Zt Liu by Senior III
  • 6305 Views
  • 11 replies
  • 0 kudos

CMSIS compliant drivers STM32

Posted on May 14, 2014 at 13:44Hi,Currently i am working on a code refactoring project, my first requirement is to use CMSIS driver library for replacing existing driver library(developed by us) so that incase of a microcontroller change in the futu...

vijith by Associate II
  • 5094 Views
  • 7 replies
  • 0 kudos

STM32F407 USB MSC example code

Posted on October 23, 2017 at 14:00I am looking at running USB Host software on the STM32F407VG device, probably using the STM32F407G-DISC1 eval board but haven't ordered it yet.I downloaded the STM32_USB-Host-Device_Lib_V2.2.0 example code from the...

STM32F4 - SDIO FAT write problem

Posted on June 21, 2017 at 14:26Hi community!To replicate my setup you need:- discovery (F407)- Discover - M0 expansion 'shield'- Sd Card- download my test project under atollic here (cube mx project included):    https://uloz.to/!mbYhN53eRdyf/cubem...

How does HAL_I2C_IsDeviceReady work?

Posted on October 19, 2017 at 20:38 Hi all, I'm dealing with an I2C memory connected to a STM32F401 MCU and I'd like to check at runtime if the device is ready (or if something is wrong, e.g. with wirings). I'm trying to use the HAL_I2C_I...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.