STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32Cube LwIP TCP Sending

Posted on April 12, 2018 at 15:49I have used the STM32Cube software and the tcp_echoserver to create a working echo server with no issues. Now I am trying to expand on the echo server. I want to be able to send data without the requirement of data h...

Touch Sensing channels count STM32L152ZE

Posted on April 12, 2018 at 12:30 Is there a error in theSTM32_TouchSensing_LibraryV2.1.1 with the maximum channel count for theSTM32L152ZE controller. According to theUM1913 usermanual the STM32L1xx supports up to 34 channels. STM32L1 seri...

Resolved! I want to write and read data from M24M01-RMN6TP (EEPROM) by using STM32F427ZITx processor, please help me?

Posted on April 10, 2018 at 12:49I DON'T KNOW ADDRESS OF M24M01-RMN6TP slave.if((HAL_I2C_Master_Transmit(&hi2c1,(devAddess),(uint8_t *)&buffer,3,100))==HAL_OK){ HAL_GPIO_TogglePin(GPIOF,GPIO_PIN_4); HAL_Delay(200);}if((HAL_I2C_Master_Receive(&hi2c1,...

Resolved! STM32L4 - LL_USART_TransmitData8 trigger RXNE

Posted on April 10, 2018 at 14:27 Hello, I am having a problem with RX interrupt. Everytime I callLL_USART_TransmitData8() it triggers RXNE flag. I enabled only RXNE , ERROR and disabled TXE. Also, If I send bytes to UART does not trigger RXNE...

USB Host CDC support to FTDI Devices

Posted on October 08, 2014 at 09:20Hi, has anyone tried communicating USB Host CDC/VCP to FTDI devices ( Chip FT232R )? which is a vendor specific class implementation. we are trying that with STM3220G eval to communicate with some FTDI based device...

lokesh by Associate II
  • 5381 Views
  • 8 replies
  • 0 kudos

FreeRTOS+TCP NetworkInterface Porting

Posted on April 10, 2018 at 16:05I'm trying to to port the NetworkInterface.c to STM32H7 I'm following the instructions provided forhttps://www.freertos.org/FreeRTOS-Plus/FreeRTOS_Plus_TCP/Embedded_Ethernet_Porting.htmlfor other chips.As for first s...

stm32L151ZCTx ADC channel

Posted on April 09, 2018 at 14:10As STM32L151ZCTx has 40 adc. There are two banks to select adc channels for conversion. In CubeMX, ADC can have only one bank selected at a time. I have following questions:1) BANK A has 29 channels, But cubeMX shows...

Hobbyist by Associate II
  • 1288 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.