STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! F767ZI issue using IAP with Dual Bank Flash

Posted on February 10, 2018 at 00:46 Im Using STM32F767ZI Nucleo Board which has 2Mbytes of flash for code storage. It also allows for the flash to be evenly divided between two banks. This gives bank 1 one Mbyte of data, and bank 2 one Mbyte of ...

0690X00000609f7QAA.png 0690X00000609fCQAQ.png
ayarema by Associate II
  • 7598 Views
  • 12 replies
  • 0 kudos

One Pulse and HAL_SPI_Receive

I am using soft pulse triggering via "__HAL_TIM_ENABLE(&htim1)" but have a problem with the code shown below.HAL_TIM_OnePulse_Start(&htim1, TIM_CHANNEL_1);volatile uint16_t array [300];HAL_Delay(1000);      // let ADC power up      while(1)       {  ...

SSmit.0 by Associate II
  • 1730 Views
  • 3 replies
  • 0 kudos

STM32F4 I2S clock configuration for stereo PDM

Hi guys,I have an STM32F412 discovery board and am attempting to find the best solution for connecting 8xPDM microphones in 4xStereo pairs and writing the resulting WAV to USB. The method I'm currently attempting is:Use 4xI2S peripherals, each with 2...

0690X000006CDC5QAO.jpg 0690X000006CDCKQA4.jpg
sully by Associate II
  • 2949 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F103C8T6 TIM1 interrupt not occuring

I would like to have an interrupt every second on my TIM1 I use a STM32F103C8T6Here is my timer init:  static void MX_TIM1_Init(void) {   TIM_ClockConfigTypeDef sClockSourceConfig; TIM_MasterConfigTypeDef sMasterConfig;   htim1.Instance = TIM1...

paul sauv by Associate III
  • 1400 Views
  • 1 replies
  • 0 kudos

How to send message via Tx?

Hi All;I would like to send 464a2f5e via HAL_UART_Transmitt. I am use tochar UDPBuffer[512]; uint8_t X = 0;   UDPBuffer[X++] = 0x4e; UDPBuffer[X++] = 0x4a; UDPBuffer[X++] = 0x49; UDPBuffer[X++] = 0x4f; UDPBuffer[X++] = 0x54; UDPBuff...

Gz by Senior
  • 1936 Views
  • 4 replies
  • 0 kudos

STM32 Boot options

Hello every i am trying to explore booting sequence of STM32 MCU STM32 has three boot options 1)Boot from user Flash 2)Boot from system memory 3)Boot from embedded SRAM. What is ment by system memory..?Thanks in advance

Njore by Associate
  • 1519 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.