STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using PDM to PCM conversion library

I am using a STM32L1 MCU and I want to use the PDM to PCM conversion library, so I downloaded X-CUBE-MEMSMIC1, in the audio PDM lib folder I found libPDMFilter_CM3_Keil.lib. In the release note I read this lib is for 16KHz PCM data sampling rate, So ...

J Lee by Associate III
  • 5092 Views
  • 4 replies
  • 0 kudos

Resolved! STM32L4 USB PID Allocation for consumer product

Hi,I am working on a consumer product based on STM32L4 microcontroller and need to register a new PID before we start shipping. Appreciate some assistance.Similar threads:https://community.st.com/s/question/0D50X00009XkXJESA3/help-needed-with-usb-pi...

CPatr by Associate
  • 1887 Views
  • 3 replies
  • 0 kudos

Resolved! STM32F042 Bootloader Activation

Hy, I am planning a system where 2 STM32F042 UFQFPN28 devices serve as CAN Controller and are controlled by one master CPU. PCB Space and CPU pins are short. I need to guarantee a fail safe FW update for the two STM32 MCUs.I plan to wire the system a...

0690X000006CGl8QAG.png 0690X000006CGlIQAW.png
harald by Associate III
  • 2078 Views
  • 4 replies
  • 1 kudos

Any USB examples for the NUCLEO-H743ZI board?

I could not find any in the Cube packages... I tried creating a project from scratch with STM32CubeMX. Power for USB FS1 is ready (LD10 on) but no reaction at all when I connect anything via user USB port (CN13). The same project works on the STM32H7...

Microman by Associate III
  • 1343 Views
  • 2 replies
  • 0 kudos

STM32F103C8 USB Unknown Device Problem

Posted on July 27, 2017 at 15:51Hi friendsI am trying to make usb hid connection with STM32F103C8. I was able to compile the USB Library via the KEIL Compiler. The processor is running. After the USB init routines, the processor goes to the main pro...

0690X00000603ywQAA.jpg

USB device not enumerating sometimes

Posted on January 06, 2015 at 08:13We are using STM32L151CBU6 in our product development and need to connect the device to PC over USB. I have used the USB driver provided by ST. I am seeing a really strange and frustrating behavior. From the IAR de...

pankaj1 by Associate
  • 1423 Views
  • 1 replies
  • 0 kudos

STM32F4 Write To USB3.1 Get Problem

I am using STMF4 USB function to log data, it can write readable data file to USB2.0. But it gets problem with USB3.1, when I write a log file to USB3.1, and open it with PC, PC report "the file or directory is corrupted and unreadable".Does any one ...

STM32F769 SDMMC corruption with Ethernet DMA?

Hi,On STM32769NI EVAL board I have LWiP running the ethernet port. This is a merge of two pieces of example code that come with the Cube.I also have SDMMC being read by FATfs.Prior to adding Ethernet, all was well. Now, calls to HAL_SD_ReadBlocks_DMA...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.