STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HAL_Delay() not working properly?

Hi,I'm working on a project to create a voltage inverter controlled by a STM32103C8T6 (the bluepill). Later, I intend to include a boost converter to have a better voltage control.The problem is that my delays aren't working properly. Where I should ...

Battery Charge Detection Fails after First Time

I am having a similar problem to this post: https://community.st.com/s/question/0D50X00009XkewvSAB/battery-charging-detectorusbbcdr-of-stm32f04-only-works-one-timeThis is on an STM32L433 using L4 HAL 1.13.0.Initially, all subsequent BCD checks after ...

Resolved! STM32L4 reference manual usb sram adress discrepancy

Dear Sir or madam, I would like to report a discrepancy in the reference manual of the stm32l4 series Quote from 45.6.2 Buffer descriptor table "The first packet memory location is located at 0x4000 6000"The package memory for usb is also called usb ...

ThiZi by Associate
  • 1665 Views
  • 3 replies
  • 0 kudos

HAL: Unused parameter warnings

I compile my code with -Wunused-parameter and I get many "warning: unused parameter …" for the STM32F4 HAL.Would be great if this can be fixed in the library. I don't want to change the library and then have to maintain the changes.Thanks!Harjit

stm32f429zi nucleo ethernet socket

I am working on stm32f429zi nucleo board on ethernet .1) Is it possible to implement SOCKET programming without RTOS.(if so any source code available)2) Any resource for implementing standalone TCP data transmit and receive.(any source code available...

KINGame by Associate III
  • 672 Views
  • 0 replies
  • 0 kudos

HAL I2S timeout error

HAL I2S timeout error, look at my code below, i had it working one day and now it never works, the HAL_I2S_Receive function is only called once and then I run into HAL_StatusTypeDef being stuck in HAL_TIMEOUT.while (1)   {   /* USER CODE END WHIL...

uahma by Associate
  • 1766 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.