STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ethernet receive stability using TCP

Receiving TCP stream that spans two packets fails after several seconds. Pings still work. The STM32F7 replies to the receive stream with duplicate ACK'sThe TCP stream does not recover.Ethernet Receive Logic Review using STM32Cube_FW_H7_V1.3.2/Proj...

STM32F030K6T6 Timer 1 PWM CH2N not Working

Hello everyonei using Timer 1 and set PWM on CH1 and CH2N CH1 is work fine but CH2N not working (i checked pin work fine on nromal GPIO)my code only have two line :HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_1);HAL_TIM_PWM_Start(&htim1, TIM_CHANNEL_2);any...

Pedram by Associate III
  • 2295 Views
  • 2 replies
  • 0 kudos

HAL SAI transfer I2S on STM32F469I-Disco

Hi, how do i send data to the CS43L22 codec on the board? In the audio example, it sends 16bit uint values with the eval_audio_play, but on the HAL_SAI_transmit functions i can only send 8bit values. I cannot find a solution, i configured the DAC and...

Deividas by Associate II
  • 985 Views
  • 0 replies
  • 0 kudos

Known issues with STM32 USB CDC?

HiI use the STM32L452 configured as a USB CDC device which is connected to a host PC.Once every 1-2 weeks the communication breaks down in the OUT direction as seen from the host.In other words the host receives data, but it's not able to send anythi...

abaldur by Associate III
  • 2879 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.