STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

FP-AUD-AEC1 Hard Fault on STM32WB55REV

Hey everyone,I'm currently trying to integrate the STM32 FP-AUD-AEC-1 software package in a multithreaded environment (ThreadX) on an STM32wb55rev7 mcu chip. Library compiles and runs but eventually hard faults during thread initializations. Any advi...

coop6 by Associate
  • 538 Views
  • 2 replies
  • 0 kudos

SDRAM FMC with STM32H7

Hi everyone, my custom board previously had an STM32F746BGT6. Since we were looking for a microcontroller with a graphics accelerator, we opted for the STM32H743BIT6 (which is pin-to-pin compatible). All the peripherals work, but I'm having trouble i...

Giovanni3 by Associate III
  • 1581 Views
  • 10 replies
  • 0 kudos

Static DFU Serial Number on STM32F723xx

There have been previous posts about determining how the DFU serial number is formed from the 96-bit Unique ID.  However, when using the ROM bootloader for the STM32F723xx MCU I don't see unique serial numbers at all.  I am always seeing the same DFU...

jwj by Associate
  • 624 Views
  • 2 replies
  • 0 kudos

PDM Mono Mic on SAI_A with DMA Transfer

Hi, this is my first post here and one of my first experiences with the STM32.I'm working on an STM32H7A3ZI-Q development board. I've connected an Adafruit PDM microphone to SAI1_A with clock on PE2 (SAI1_CK1) and data on PE6 (SAI1_D1). I'm not an ex...

Immagine.png Immagine2.png Immagine3.png
LGR by Associate
  • 685 Views
  • 1 replies
  • 0 kudos

STM32U5A5 instruction fault after WFI

Struggling with a really weird issue here. I'm working on a project using Zephyr on an STM32U5A5ZJT6Q. We are using an LSE-clocked LPTIM as the tick source, PM enabled with STOP0 and STOP1 modes.At some point, we started noticing random crashes, whic...

kamnxt by Associate
  • 545 Views
  • 0 replies
  • 0 kudos

DCMIPP silient failure

Hello team, Another day,  new same issue. :pensive_face:I have setup the DCMIPP PIPE 1 for the stm32n6570 DK, so that it dumps frames in address 0x34200000 which maps to SRAM3 begin address I have enabled bothe the memories SRAM3 and SRAM4 but with o...

KamurasiJordanArthur_2-1761801451579.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.