STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! [SOLVED] CAN callback never call

I'm working on an STM32L431 and I never be call on HAL_CAN_RxFifo0MsgPendingCallback. I have set a break point in this function but the debugger never stop on it.In my program:I have generated the code using CubeMx and I set NVIC on CAN1: Tx, RX0, RX...

AJouv by Associate II
  • 2142 Views
  • 4 replies
  • 0 kudos

STM32L432KC Nucleo32 board VCP with Android

I am failing to get a project based on the STM32L432KC Nucleo32 board to communicate with an Android device via USB VCP.The Nucleo project works fine over USB VCP on Windows and Linux. And a similar STM32L433-based device I made using CDC works fin...

pwm complementery pins state once we stop pwm.

HELLO,I am trying to implement h bridge logic to convert dc to ac but i am not sure about the pin states of complementery pwm once it stop pwm on that and how to use those compl. pwms pins as gpios .what i am actually trying to achieve is run compl p...

Akhan.4 by Associate II
  • 2437 Views
  • 5 replies
  • 0 kudos

Simple multi-user http server

Hello! Recently, a stm32 microcontroller came to me and I want to make an http server. On the Internet, looking for projects on stm32 using the lwIP library. But I can not find a multi-user http-server for my device. Some programs after a while begin...

STM32F746ZG Nucleo / Lwip problem

Hallo,My board is the STM32F746ZG Nucleo board.I am using the LWIP_HTTP_SERVER_NETCONN_RTOS example from the stm32cubef7 package.The example works fine initially but if I leave it running for several hours suddenly the board stops responding in any h...

STM32H743ZI Ethernet LWIP TCP Echoserver

Sorry for my bad englishHi.I use STM32H743ZI and develop firmware.I put an example of a lwip tcp echoserver in my firmware.Example: STM32H743ZI-EVAL lwip tcp echoserver applicationI'm not using RTOS.My question: Ethernet operation relies on build opt...

KKim.19 by Associate II
  • 719 Views
  • 0 replies
  • 0 kudos

STM32F103 STD Periph I2C help

Hi,I want to send 2-bytes from I2C in a single transaction with std peripheral library. For 1-byte i can handle with code below, but how can i send 2 bytes ? Any advise ?void I2C_Write_Byte(I2C_TypeDef* I2Cx, uint8_t reg_addr , uint8_t reg_data, uint...

er3481 by Senior
  • 816 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.