STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32CubeMX + CAN + HAL

I have a STM32F373VCT6 MCU with CAN bus connected to PD0 and PA12 pins. I also have an old project which have these pins configured by hands and CAN bus works properly for this project. Now, I need to create new project for this MCU and I try to do i...

Empty STM32L4R5 (with factory default settings) will try peripheral boot through system memory no matter what (bug?). PA9 then becomes output (as USART1_TX). Shall we use a resistor for VBUS?

Strangely an empty STM32L4R5 will try to boot from system memory and then will try all peripherals turning GPIOs to outputs while trying. Of course this is very dangerous if not taken into account in the design of boards that are to be started with "...

Resolved! Hi, I'm using stm32L073Rz , need to know how to configure it as a usb memory device, no demo examples are available for usb memory stick for this chip , i used cubemx to generate code for usb memory class and ran it.

It does not work , it gets detected as unknown device,what am i missing , should i add something more to cube mx generated code. Thanks.

svii by Associate III
  • 1631 Views
  • 3 replies
  • 0 kudos

stm32l476 disc uart DMA not working

#include "main.h"#include "uartDma.h"UART_HandleTypeDef huart2;DMA_HandleTypeDef hdma_usart2_tx;void uartStart(void){ MX_DMA_Init(); MX_USART2_UART_Init(); uint8_t pData[] = "This is Polling\r\n"; uint8_t pdata[] = "This is Dma\r\n"; HAL_UART_Tran...

Jagath by Associate II
  • 760 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.