STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Read USB camera with MSC usb

Hi,I have a request from a client to take photos(from a camera) at a fixed time (timelapse) and send to the cloud.My idea would be to load photos from the device via USB with an STM32.I tried a USB example MSC Host with my STM32F746-Disco kit.With a...

PCu1 by Senior
  • 1922 Views
  • 5 replies
  • 0 kudos

Doubts about the inconsistency of bit width between ll library and standard library timer input capture return value data

Hello everyone, when debugging, we found that the input capture return value of ll library is different from that of standard library. Ll library forces the return value to 32-bit, which is originally only 16 bit, as mentioned aboveCapturedvalue (bet...

0693W000000UfbXQAS.png 0693W000000UfbwQAC.png
仕陈.1 by Associate
  • 1809 Views
  • 3 replies
  • 0 kudos

STM32G4 HAL manual doesn't cover the I2S API.

Hi ST supportThe "Description of STM32G4 HAL and low-layer drivers" ( UM2570 rev 1.0) doesn't cover any I2S HAL API ( HAL_I2S_* ). The manual can be downloaded from here :https://www.st.com/ja/embedded-software/stm32cubeg4.html#resourcePlease check a...

Takemasa by Associate III
  • 1651 Views
  • 3 replies
  • 0 kudos

32F411EDISCOVERY

I already bought 32F411EDISCOVERY and programmed it with my simple program. Where can I download the original firmware, which was with the purchase (it is not on the download page)?

PIvan.3 by Associate
  • 2467 Views
  • 6 replies
  • 0 kudos

Resolved! STM32G474 Nucleo. Overclock example for HRTIM problem

I compiled example from st cube. I found in clock configuration this parameters:RCC_OscInitStruct.PLL.PLLM = RCC_PLLM_DIV6; RCC_OscInitStruct.PLL.PLLN = 85;This give to sysclk 177Mhz and it exceeds max frequency... when I set parameters to:RCC_OscIni...

MSzaj.1 by Associate II
  • 2225 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.