STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

DFU file manager

Good morning,I'm working with STM32L4 and I have created my own bootloader.In order to program the MCU, I use USB interface, so I need the DFU file. I use the 'DFU File Manager' tool to create the DFU file from the HEX file. It works fine, but then, ...

Resolved! NUCLEO-H745ZI-Q unable to enumerate FS USB device

Hello,I have a NUCLEO-H745ZI-Q board that I am trying to configure as a FS USB device setup as a Virtual Port Com. The only changes I have made to the stock CubeMx setup is removing ETH and setting up two encoder inputs on TIM2 and 5. I've tried disa...

SPetr.6 by Associate III
  • 1068 Views
  • 1 replies
  • 0 kudos

Ethernet frame length issue

Hi, I got a problem when I use the Ethernet TCP stack and hope someone can help me figure it out.I am using tcpecho protocol to communicate between PC and the board. PC send the command and board response with the data. If I just send 64 bytes, as: ...

kqian by Associate II
  • 3092 Views
  • 5 replies
  • 0 kudos

STM32F746 Discovery board USB MSC example

hello,we would like to run USB MSC example using STM32CUbe IDE toolsSTM32IDE V1.3HAL V1.16hardware STM32F746 Discovery boardUsing Internal USB PHY, 12 Mbit.we start with demo applications located \\STM32Cube\Repository\STM32Cube_FW_F7_V1.16....

IB.1 by Associate III
  • 1127 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.