STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VENC_SDCard_ThreadX Example

Hi, @krastThe readme for the VENC_SDCard_ThreadX examplehttps://github.com/STMicroelectronics/STM32CubeN6/blob/main/Projects/STM32N6570-DK/Applications/VENC/VENC_SDCard_ThreadX/README.mdstates:"The output is raw since no file system is used for now"b...

Resolved! STM32F407VET6 Black Pill V2

I procured an STM32F4VE 2.0 board *Details of board here:*https://stm32-base.org/boards/STM32F407VET6-STM32-F4VE-V2.0I managed to create a Basic STM32 Cube Project for this controller. (STM32F407VET6)From the Schematic on STM32base website, I see PA1...

nagendra_1-1764608023780.png nagendra_2-1764608076266.png nagendra_4-1764608204186.png nagendra_0-1764607947951.png
nagendra by Associate
  • 951 Views
  • 2 replies
  • 1 kudos

Resolved! Error in PSSI HAL code for HAL_PSSI_Abort_DMA

I am working with an STM32U575, HAL version 1.5 and found the issue described below(Have checked the HAL code for the H5 and H7 and these contain the same issue)See picture below, when aborting an PSSI transfer, before checking the state on lines 125...

LVan31_0-1718625311115.png
LVan .31 by Associate III
  • 1847 Views
  • 3 replies
  • 1 kudos

Bug in example of NUCLEO-U575ZI DAC&DMA?

Hi, there is this example for using the DAC with DMA for the NUCLEO-U575ZI:https://github.com/STMicroelectronics/STM32CubeU5/tree/main/Projects/NUCLEO-U575ZI-Q/Examples/DAC/DAC_SignalsGeneration_DMAIn the current V1.2.0 of file https://github.com/STM...

psfahr by Associate II
  • 384 Views
  • 1 replies
  • 0 kudos

STM32U073CC STOP MODE

HiWe are using STM32U073CC MCU in a project. Our development tools are:STM32CubeIDEVersion: 2.0.0Build: 26820_20251114_1348 (UTC) STM32CubeMXVersion 6.16.0 WE are using the HAL_RTCEx_SetWakeUpTimer_IT to wake up the mcu from stop mode. The code code ...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.