2021-08-10 12:46 AM
Hey together,
I'm switching from freeRTOS to Azure ThreadX at the moment. I know that there are problems when using newlib functions like printf with %f and so on with freeRTOS. As explained in the following link this has to do with the issue that the _sbrk implementation of ST is not reentrant. This was solved by the file of Dave Nadler:
https://nadler.com/embedded/newlibAndFreeRTOS.html
Is there anyone who has a similar working implementation for ThreadX instead of freeRTOS?
Best regards,
Eric
2021-08-15 11:18 PM
Hey together,
did anyone faced a similar problem? Wouldn't it be enough to provide an extra semaphore for the __sbrk function, get it on the entry of the function and put it on leave? I would just have to track if I am inside an ISR or not. If so I cant wait and have to leave direct, if not I could wait until the semphore gets released.
Best regards,
Eric
2021-08-26 6:53 AM
Hey together,
@Walid ZRELLI could you please raise this topic internally? I think it is very important if someone wants to use Azure RTOS. with functions like printf %f.
Best regards,
Eric
2021-08-27 2:06 AM
Hello @ESawa.1 ,
Your issue has been raised internally. I will keep you informed.
Thanks for your contribution.
BeST Regards,
Walid
2021-10-27 11:37 PM
Hey together,
@Walid ZRELLI are there any news regarding my question?
Best regards,
Eric
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.