2019-11-27 4:38 AM
When using STM32G431RBT6, Only if the filter is configured to 0 can the interrupt be entered normally, otherwise the interrupt is always not entered. AnalogWDGConfig.FilteringConfig = ADC_AWD_FILTERING_NONE.
2019-11-27 5:35 AM
Hello,
First please update your nickname to get rid of this Userxxxxx.
Then, could you please let me know which analog watchdog are you configuring?
If it is not the analog watchdog 1, then it is normal to use only the value ADC_AWD_FILTERING_NONE.
In fact, the Analog watchdog filtering feature is available only with AWD1. That is why AWDFILT bit (Analog watchdog filtering parameter) is available only for ADC_TR1 (relative to analog watchdog 1).
-Amel
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2019-11-27 5:46 AM
Hello, Amel NASRI
Thanks for your suggestion and reply.I have configured an analog watchdog 1. However, the filter can only be configured to be 0 so that it can work properly, otherwise the interrupt will not be entered (no interrupt flags will be generated).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.