2025-04-02 7:49 AM
I use JumpToBootloader() to jump to bootloader, device enters bootloader and shows device
i then send it this command
dfu-util -d 0483:df11 -S 305737513432 -a 0 -s 0x08000000:leave -D fw.bin
and device resets
Erase [ ] 0% 0 bytesdfu-util: Error during special command "ERASE_PAGE" get_status: -9 (LIBUSB_ERROR_PIPE)
If i enter the bootloader via the BOOT pin it works fine
It is like something else needs to be reset ?
dfu-util 0.11-dev
Found DFU: [0483:df11] ver=0200, devnum=44, cfg=1, intf=0, path="20-1.2.1.2", alt=0, name="@Internal Flash /0x08000000/8*128Kg", serial="305737513432"
Found DFU: [0483:df11] ver=0200, devnum=44, cfg=1, intf=0, path="20-1.2.1.2", alt=1, name="@Option Bytes /0x5200201C/01*88 e", serial="305737513432"
Copyright 2005-2009 Weston Schmidt, Harald Welte and OpenMoko Inc.
Copyright 2010-2021 Tormod Volden and Stefan Schmidt
This program is Free Software and has ABSOLUTELY NO WARRANTY
Please report bugs to http://sourceforge.net/p/dfu-util/tickets/
dfu-util: Warning: Invalid DFU suffix signature
dfu-util: A valid DFU suffix will be required in a future dfu-util release
Opening DFU capable USB device...
Device ID 0483:df11
Device DFU version 011a
Claiming USB DFU Interface...
Setting Alternate Interface #0 ...
Determining device status...
DFU state(2) = dfuIDLE, status(0) = No error condition is present
DFU mode device DFU version 011a
Device returned transfer size 1024
DfuSe interface name: "Internal Flash "
Downloading element to address = 0x08000000, size = 135828
Erase [ ] 0% 0 bytesdfu-util: Error during special command "ERASE_PAGE" get_status: -9 (LIBUSB_ERROR_PIPE)
Return Code: 74
void JumpToBootloader(void)
{
uint32_t i=0;
void (*SysMemBootJump)(void);
/* Set the address of the entry point to bootloader */
volatile uint32_t BootAddr = 0x1FF09800;
/* Disable all interrupts */
__disable_irq();
// USB->CNTR = 0x0003;
USBD_DeInit(&hUsbDeviceHS);
HAL_DMA_DeInit(&hdma_adc3);
HAL_DMA_DeInit(&hdma_dac1_ch1);
HAL_DMA_DeInit(&hdma_dac1_ch2);
HAL_DMA_DeInit(&hdma_usart2_tx);
HAL_DMA_DeInit(&hdma_usart3_tx);
HAL_CORDIC_DeInit(&hcordic);
HAL_DAC_DeInit(&hdac1);
HAL_UART_DeInit(&huart2);
HAL_UART_DeInit(&huart3);
HAL_ADC_DeInit(&hadc3);
HAL_TIM_Base_DeInit(&htim2);
HAL_TIM_Base_DeInit(&htim3);
HAL_TIM_Base_DeInit(&htim6);
HAL_I2C_DeInit(&hi2c4);
HAL_RTC_DeInit(&hrtc);
// HAL_DeInit();
/* Disable Systick timer */
SysTick->CTRL = 0;
SysTick->LOAD = 0;
SysTick->VAL = 0;
/* Set the clock to the default state */
HAL_RCC_DeInit();
/* Clear Interrupt Enable Register & Interrupt Pending Register */
uint8_t cnt = (sizeof(NVIC->ICER) / sizeof(NVIC->ICER[0]));
for (i=0;i<cnt;i++)
{
NVIC->ICER[i]=0xFFFFFFFF;
NVIC->ICPR[i]=0xFFFFFFFF;
}
/* Re-enable all interrupts */
__enable_irq();
/* Set up the jump to booloader address + 4 */
SysMemBootJump = (void (*)(void)) (*((uint32_t *) ((BootAddr + 4))));
/* Set the main stack pointer to the bootloader stack */
__set_MSP(*(uint32_t *)BootAddr);
/* Call the function to jump to bootloader location */
SysMemBootJump();
/* Jump is done successfully */
while (1)
{
/* Code should never reach this loop */
}
}
2025-05-07 7:37 AM
Hi @pmark
Check your flash string descriptor. You need to make sure that the memory paging is set up correctly.
AN3156 outlines the sequence of commands needed for successful firmware update operations.
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.