2019-01-01 7:20 AM
Hello, we are using an STM32F7 and are saving image data to USB, using mostly the BSP code (disk_write in usbh_diskio.c -> USBH_MSC_Write in usbh_msc.c and so on). However we have found it's quite slow, 6-7 seconds to save one 400x400 image.
I've started profiling and looking at the clocks (very complicated) to see if there is a bottleneck, or if this is something we will have to live with. Does anybody have any advice on improving our throughput? Thanks very much and happy new year.
2019-01-01 7:53 AM
Hi. For starters, review this thread:
https://community.st.com/s/question/0D50X00009XkeLmSAJ/usb-msc-device-low-transfer-rate-stm32f7
Some good discussion from Clive & Dr. Tsuneo Chinzei.
2019-01-01 8:02 AM
Thank you... however looks like it pertains to USB as device (transferring from PC to device?), not host (we are acting as host, saving to an attached USB stick), so there's no MSC_MEDIA_PACKET value for me to tweak. (Got my hopes way up for a second. :))
2019-01-01 8:09 AM
Are you hosting a Flash Drive?
Doing large media aligned writes helps in most mass-storage applications. For NAND arrays knowing the internal erase block size helps, but at this point is probably unhelpfully large. Allowing the "data" writes to be linear, and deferring/folding small writes to file system structures (FAT, DIR, etc) will provide a means to more optimal write speeds.
Many small f_write operations will be punishing, have a more strategic buffering scheme.
2019-01-01 8:16 AM
Thanks Clive... I am hosting a flash drive. Not sure if this is germane but I actually make just two calls to f_write, one for the BMP header and one for the entire BMP image data (400x400x3=480,000bytes). The f_write function internally loops on this about 117 times, 4096 bytes per loop, taking about 0.04sec+ per loop.
2019-01-01 8:21 AM
See here for more discussion:
https://community.st.com/s/question/0D50X00009XkYTfSAN/usbfs-msc-slow-writing-speed
and this interesting read and possible solution:
2019-01-01 8:41 AM
Thanks Mon2, I've skimmed those (Clive seems to have helped many people here :))... it actually looks like I am doing something in the *opposite* extreme, in that I am not buffering my image data *at all*, sending my entire 480000 bytes at once. From there f_write seems to split it up internally... I assume optimally? Perhaps not, I will look into how/why f_write chooses 4096 per loop. Or if you have any insight, thanks very much.
2019-01-01 8:55 AM
Sorry that I do not have any low level details of the root cause at this time but can only state that from our years of product development - we did find differences in the quality of the USB media / thumbdrives. Not all vendors are created equal. This may not be a factor but recalling that some (early) Kingston branded sticks worked well for our DOS based production cycles (using RuFUS tool) but then something changed and (recent) Kingston was on the public black list. The experience was that any PC we would use would not cold boot from the new Kingston drives - warm boot was ok but that takes away from our time to reflash each product we build. Changed to Lexar and have been happy. Boots everytime with RUFUS tool used for apply FreeDOS.
Perhaps you can test other brands of USB media? Have you tested with USB 3.0 capable drives?
Believe we have a STM32F7 kit of some sort in the lab (NOT Eval board but Nucleo) and do have a few USB bus analyzers (USB 2.0 and USB 3.1 Gen1). If if it helps, can try to set it up but as usual, limited free time when at work.
Clive - he is keeping this forum alive and very knowledgeable. Also, google Dr. Tsuneo Chinzei and check out his background and assorted patents - it is mind blowing the experience being shared from these seasoned developers.
2019-01-01 9:04 AM
Thank you Mon2, I appreciate the insight. We have tried this across a variety of sticks and we also notice differences... in fact one type doesn't write at all and we have to investigate this too. But we seem to be slow across all thumb drives.
Clive2, do you agree with my take that I am not making the same mistake as those posts? Do you think f_write should be parcelling up my buffer properly, or is something I should tweak?
Thanks both of you.
2019-01-01 9:05 AM
Agree on Clive2, he has helped me out a lot, pretty amazing how on the ball he is here.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.