2019-05-18 7:32 AM
As the title says, on a STM32F3DISCOVERY development board, if I create a fresh project with CubeMX,using OpenSTM32Workbench as an IDE, enable SWD support and FreeRTOS, but without the support for stack overflow detection in the FreeRTOS configuration, I can start a debug session and I can initially step through, but as soon as I let it run continuuously, if I then pause the target, I can not control it anymore. Connnection seems to be down then, I can't reset it, etc.
Enabling the stack overflow detection (version 2), everything works fine. So will just removing FreeRTOS. This does not seem to be because of some stack overflow since I tried also increasing the stack to quite large sizes, and I'm not doing anything anyways, it's just the clean project state.
Best,
Vlad R.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.