2023-11-17 7:23 AM
Hi all !
I want to transmit 1 bit on the SPI1 of my STM32F7.
I see that the minimum datasize to transmit is SPI_DATASIZE_4BIT. So I guess I can't send only 1 bit of data on my bus. I am wrong ?
My final goal is just to have 1 clock period on the SPI bus.
have you got any clue for that ?
Thank you for your help.
Best regards.
Remi
2023-11-17 7:38 AM - edited 2023-11-17 7:39 AM
Hi,
sorry, i see no sense . spi = serial/parallel interface ; sending 1 bit frame is nonsense here. and impossible.
explain, what you want to do - set some ws.. leds or whatever. then we can find a way to do it...(maybe)
2023-11-20 3:35 AM
Hi,
I work on a with a STM32F7 linked with a chip by a SPI bus (easy until now).
Also, the STM32F7 and the chip are linked by a pin (ouptut for the STM32, input for the chip). When the pin goes high, the signal must be "validated" by a 1 spi SCLK period (there is no direct link between this pin and the spi).
This behaviour is required by the chip...
I hope you will be able to help.
2023-11-20 3:41 AM
i cannot find my big blue glass sphere ...
so maybe better, you say which chip we talk about.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.