2024-11-08 8:41 AM
Questions:
1. How many STM32 families offer SAR 16-bit ADCs?
2. Which MCU in STM32 family is the best choice for using SAR 16-bit ADC related project with the lowest cost?
Thanks
Solved! Go to Solution.
2024-11-08 2:09 PM - edited 2024-11-09 2:59 AM
Yes you can, but NUCLEO-H753ZG is cheaper ;).
Edited: it's the NUCLEO-H753ZI But the hyperlink is correct!
2024-11-08 2:35 PM - edited 2024-11-08 2:36 PM
Also, for the NUCELO-H753ZI, we have a lot of ADC examples here.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-08 2:38 PM
I can't find " NUCLEO-H753ZG" . But there is NUCLEO-H753ZI - when you searchNUCLEO-H753ZG on Google
Are they same?
What do ZG/ZI mean?
What do H753/H723 mean?
Thanks
2024-11-08 2:39 PM
Thanks a lot
2024-11-08 2:42 PM - edited 2024-11-08 2:48 PM
This is just a typo from my college @mƎALLEm .
For the H753/H723, H is the Product type with H = High performance and 723/753 is the device subfamily. You can find it explained on the Ordering information of each datasheet of an MCU.
Hope you enjoy our support.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-08 3:47 PM
2024-11-08 10:23 PM
For the naming of the MCU, PLease refer to the Ordering information chapter of each MCU on a board. For the price it should be normal since the STM32H7S3 is the newest product on the STM32H7 Familly (just released on march 2024).
This post became so long and we are not tooking anymore about the original topic. So please close it by selecting a best answer for it(using the accept as solution button). The best answer should be the comment that answer your original request.
For your comming questions, you can add new posts to the ST Community and we will be happy to help.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-11-09 2:18 AM - edited 2024-11-09 2:57 AM
@RongShengWang wrote:
There are two under H753NUCLEO-H753ZI and NUCLEO-H7S3L8What is the difference between the two?
You need to refer to the related datasheets to get the differences.
@RongShengWang wrote:
Why NUCLEO-H7S3L8 costs $9+ more than NUCLEO-H753ZI?
Please contact your local sales for that question.
@RongShengWang wrote:
Which one has the better noise immunity?
For that question related to EMC / EMI please submit ols ticket: https://ols.st.com/
Thank you
2024-11-09 8:45 AM
SAR ADC in STM32H7S3 has ONLY 12-bit.
SAR ADC in STM32H753 has 16-bit.
We need 16-bit.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.