2025-02-13 2:26 PM
Hello,
I am a PowerTrain Electronics Hardware Architect by profession.
For one of my new hobby electronics developement I decided to use STM32 micro controller.
To start with I bought NUCLEO_F030R8 and able to blink on board LED as I program.
Then I tried to program on board micro controller with my ST-LINK/V2 ISOL. I disconnected both jumpers at CN2. Tapped out SWCLK of target controller from pin 2 of CM6. Then tapped out SWDIO from pin 4 of CN6. I took 3.3V and GND from CN6 pins 4 and 6 respectively. I connected these four wires to ST-LINK/V2 ISOL as in the image
In Debug configurations of CubeIDE, ST-LINK/V2 ISOL is founf with SWD setting. But when I try to program I get error message as target not found.
What am I missing here? Is the reset is mishandked by onboard programmer? Should I take care of this and few others?
Thank you, Anesh S.
Solved! Go to Solution.
2025-02-16 11:35 AM
Hi,
As you mentioned O have changed the SWD connections to C7. But I have not used correct GND pin from STLINK-V2/ISOL. I wrongly connected Pin 19 of STLINK-V2/ISOL which is NC. I changed GND to Pin 18 and now I am able to program the Nucleo board with STLINK-V2/ISOL.
Now I can confifently proveed my own hardwrae design with STM32 micro controllers with SWD port for programming and debugging.
I request ST to provide a connector/Cable for STLINK-V2/ISOL to easilz connect SWD pins alone to the target board.
Thank you so much, With best regards, Anesh S.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.