2011-07-05 5:20 AM
Hi, I am new to this and trying to get my STM32 Discovery board working with the Atollic IDE. I'm following the instructions for this board/IDE combination in the PDF files provided by the manufacturer, but I am running on a 64-bit version of Windows 7 which isn't listed in their set of requirements.
I get as far as clicking the debug icon in the IDE, the gdbserver launches and fails with this message:
Starting server with the following options:
Persistant Mode : Disabled
LogFile Name : debug_log.txt
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Error in Initializing ST-Link device
Note that SWD debug is enabled, as this not being so seems to be the most common issue for this failing.
I can connect to the board using the ST-Link utility v2.0, and it shows me the correct device info.
Is Windows 7 compatibility the issue? Is there something I need to do to the STM 32 board to get it to play ball?
Any suggestions gratefully received!
#st-link-gdbserverWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.