STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Do not connect the PC to the ST-LINK (CN7) when R30 is soldered. The PC may be damaged or the board may not be powered correctly.

In the data sheet of STM32L4, it cautions me that "Do not connect the PC to the ST-LINK(CN7) when R30 is soldered. The PC may be damaged or the board may not be powered correctly.". But I found that R30 has benn soldered when i got it. What should i ...

lzhij.2 by Associate II
  • 2294 Views
  • 2 replies
  • 0 kudos

STM32F103 stuck at boot0

I have a system based on STM32F103 microchip. It has a PCB boot0 pin which is used only when flashing new firmware. During the daily usage of the system, the PCB boot0 is not connected to anything. I have always connected to 1.5 Volts input in order ...

_legacyfs_online_stmicro_images_0693W00000bhlktQAA.png
ACher.10 by Associate II
  • 7702 Views
  • 5 replies
  • 0 kudos

ST-Link cable length

Hello,does anyone know what the maximum cable length is for the ST-Link programmer (20-pole ribbon cable)?Maybe someone has experience with this?Is it possible to bridge longer distances, e.g. 50 metres? (not the USB cable, but the 20-pole ribbon cab...

Moritz1 by Associate III
  • 7108 Views
  • 10 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.