2025-11-11 2:07 AM
I am currently working on a new hardware design using the STM32U575VIT6 (LQFP64, 10 × 10 mm) microcontroller.
I would like to request:
Reference schematics and layout guidelines for STM32U575 in LQFP64 package
Recommended power supply and decoupling capacitor design
Crystal oscillator and reset circuit design guidelines
Any available design checklists or application notes
My design overview:
,low-power IoT sensor node
Peripheral interfaces planned: SPI, I²C, ADC, etc.
Kindly share any relevant schematics, PCB layout examples, and design documentation to ensure proper implementation.
Thank you very much for your assistance.
Thanks
Harshith
Solved! Go to Solution.
2025-11-12 12:54 AM
There is not any evaluation board or official reference schematic based on the STM32U575VIT6 MCU. So, the best reference is the hardware design guide I’ve already mentioned.
Best Regards.
II
2025-11-11 3:21 AM
2025-11-12 12:50 AM
Hi @Issamos
I have Referred ,i did not got the any schematic of this STM32U575 in LQFP64 package Pls share the guidance schematic if you have .
thanks
2025-11-12 12:54 AM
There is not any evaluation board or official reference schematic based on the STM32U575VIT6 MCU. So, the best reference is the hardware design guide I’ve already mentioned.
Best Regards.
II
2025-11-12 1:40 AM
Yeah, Much Thanks.
i have one more Doubt ..
Am planning to Quad SPI, which port we can use, i cannot able to find the data sheet below listed pins can use
Controller -STM32U575VIT6 (LQFP64, 10 × 10 mm)
2025-11-12 1:45 AM
This is a new question. So, to give it more visibility, I suggest you to select the answer of the original question of this post as best answer and to create a new post on the STM32 MCUs Forum to have more chances to be answered by the community.
Best Regards.
II
2025-11-12 1:48 AM
2025-11-12 1:51 AM
Am planning to Quad SPI, which port we can use, i cannot able to find the data sheet below listed pins can use
Controller -STM32U575VIT6 (LQFP64, 10 × 10 mm)
2025-11-12 3:03 AM
Please select the answer of this post too since it is answered also.
Best Regards.
II
2025-11-12 4:41 AM
New thread for the new question is here:
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.