2024-03-26 7:51 AM - edited 2024-03-26 5:52 PM
Hi Community,
I am currently facing an issue with my STM32H7B3I-DK board. The board was working fine, but suddenly, while I was uploading the code, the LD7 LED turned on indicating a low voltage fault. However, I am confident that the USB is providing the correct voltage.
In an attempt to resolve the issue, I tried upgrading the firmware and used CubeProgrammer to reset the board with a shown voltage alternating between 0.21v, 0.35v and 0v. I also tried using the STLink utility, but I keep getting the “No STM32 Target found” error, and there is a Fail File existing in the mass storage when connecting the board containing "The interface firmware FAILED to reset/halt the target MCU".
Additionally, I noticed that the WiFi LED (LD1) and the 5V Power LED (LD5) are weakly lit. I am unsure if this is related to the current issue or if it’s a separate problem.
I have been searching for solutions online and tried several suggested methods, but none have worked so far. I would appreciate any help or suggestions on how to resolve these issues.
Troubleshooting Steps Taken:
Current Issues:
Board Details:
I hope it's not a faulty hardware component, I appreciate any assistance!
Solved! Go to Solution.
2024-03-30 5:41 AM
2024-03-26 9:54 AM
That does sound like a lot of inadvisable actions.
The ST-LINK Utilities predate the STM32H7Bx, so wouldn't be using that for any predictable out come.
Might suggest strapping BOOT0 to ground, power cycling the board completely a couple of times, and them trying to connect and mass erase using STM32 Cube Programmer
Perhaps consider what you were doing when it failed, perhaps incorrect LDO/SMPS settings, of VOS settings. Board siting on a conductive surface, or other connectivity which might has caused shorts, or high voltages from external sources.
Review the schematic, see if you can check voltages / expectations at various points.
2024-03-26 5:14 PM
@Tesla DeLorean Hi, thank for replying, The board doesn't provide access to boot0 pin externally, I saw the schematic as you said, I found where it is situated but I can't strap it to ground, Do you think there is another solution ?
2024-03-30 5:41 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.