2025-06-12 7:50 AM - last edited on 2025-06-12 7:56 AM by Andrew Neil
Hello,
I will need some help to determine if STM32H735G-DK STMOD+ connector Pin 4 SCK/RTS can be configured as a GPIO pin. Not sure which port is mapped to this pin as I will need to control this pin as a GPIO.
Thanks.
2025-06-12 7:55 AM - edited 2025-06-12 7:55 AM
@gila2025 wrote:Not sure which port is mapped to this pin .
The schematics, as always, are on the 'CAD Resources' tab of the board's Product Page:
https://www.st.com/en/evaluation-tools/stm32h735g-dk.html#cad-resources
Also check out the User Manual - available on the 'Documentation' tab:
https://www.st.com/en/evaluation-tools/stm32h735g-dk.html#documentation
2025-06-12 8:43 AM
According to UM2679 (https://www.st.com/resource/en/user_manual/um2679-discovery-kit-with-stm32h735ig-mcu-stmicroelectronics.pdf, "8.4 P2 STMod+ connector") the wiring of some pins on STMod+ depends on solder bridges.
Pin4 is routed via SB6 (default: closed) to PF8 and via SB7 (default: open) to PF7.
So with an unmodified DK pin 4 can be used as GPIO PF8 (if not used as U(S)ART7_RTS). Opening SB6 and closing SB7 moves pin4 to GPIO PF7 (alias SPI5_SCK).
(Table 15 in UM2679 is a bit misleading since the default configuration for pins 1 through 4 is not mentioned first but second.)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.