2025-01-17 2:29 PM
I have attached herewith the first iteration of the schematic for my custom stm32 board utilizing the H753ZIT6 MCU.
I would like to clear few doubts regarding
1) In the nucleo schematic for the same, STM has used F7 MCU for their ST Link interface, should I do the same? or rely on SWD/JTAG for boot and programming.
2) I am evaluating between choosing either JTAG or SWD for my main means of communicating with the IC, should I make provision for both of these on a single connector?
3) If I am choosing not buy the STLINK V3 or V2, what do I need to take care of, from both a hardware and software point of view?
4) The oscillators chosen are: TSX-3225_24.0000MF20G-AC0 for HSE and CM8V-T1A-32.768k-9pF-20PPM-TB-QA for LSE. Is their respective circuitry correct and in general the chosen oscillators right? I read the AN2867 guide but most of the recommended oscillators were over-budget for my specific project.
This is my first time ever being involved in hardware design, so if any common mistake is found, please let me know.
Thank You
2025-01-17 3:02 PM - edited 2025-01-17 3:10 PM
> 1) In the nucleo schematic for the same, STM has used F7 MCU for their ST Link interface, should I do the same?
If you want to have a ST-LINK available for your product, provide a connector for external ST-LINK (or other adapter such as J-Link), or mount a suitable ST-LINK v3 onto your board. You cannot just use a normal STM32F7 because the firmware for ST-LINK is not available to you. For the external clock (HSE) - better use a normal crystal or oscillator.
2) depends on your requirements. If no requirement - do what is easier (SWD).
> 3) If I am choosing not buy the STLINK V3 or V2, what do I need to take care of,
Just provide a connector for external adapter (maybe with some UART routed to the debugger VCP).
> most of the recommended oscillators were over-budget for my specific project.
Then correct the budget, before it's too late? By the way. under-estimating the cost is a common beginner mistake )) Always have a safe margin.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.