2024-09-11 9:32 PM
hi,
i am Using STM32G0B1RCT6
USB_CLK = 48MHZ
USB_DRD_FS---Host_Only_FS,
USB_HOST---Mass Storage Host Class,
FATFS---USB Disk
USB Interrupt---Enable
If you set it to the above mode and operate it, the USB is recognized and i configured PB4 as an output, which is connected to a green LED. Whenever I plug in the USB to my controller, the green light appears, and whenever I remove the USB from the controller, the green light turns off. so usb detected successfully, but the USB Mount/Unmount function does not work.
It works fine with stm32f429zit6 with same configuration. What causes it? how to solve this problem?
static void USBH_UserProcess (USBH_HandleTypeDef *phost, uint8_t id)
{
/* USER CODE BEGIN CALL_BACK_1 */
switch(id)
{
case HOST_USER_SELECT_CONFIGURATION:
break;
case HOST_USER_DISCONNECTION:
Appli_state = APPLICATION_DISCONNECT;
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4, RESET);
Unmount_USB();
break;
case HOST_USER_CLASS_ACTIVE:
Appli_state = APPLICATION_READY;
HAL_GPIO_WritePin(GPIOB, GPIO_PIN_4, SET);
Mount_USB();
Check_USB_Details();//check Space Details
Scan_USB("/");//Scan for files and Directories
Create_File("/ROOTFILE.csv");
char csv_data[] = "Name, Age, Salary\n\nBerlin, 27, 60000\nAlice, 28, 55000\nAlbert, 32, 55000\n";
Write_CSV_File("ROOTFILE.csv", csv_data);
break;
case HOST_USER_CONNECTION:
Appli_state = APPLICATION_START;
break;
default:
break;
}
Solved! Go to Solution.
2024-10-25 9:12 AM
It seems you have custom implementation of Mount_USB() Unmount_USB() and they are not defined. Would you mind clarify?
Did you try the example using FatFs
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2024-10-25 9:12 AM
It seems you have custom implementation of Mount_USB() Unmount_USB() and they are not defined. Would you mind clarify?
Did you try the example using FatFs
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.