cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F777 1.125 Volt on VCAP

bassetteporn11
Associate II

Is this a normal reading?

Havent installed ALL caps yet. I think I had bad contatc between SWCLK and connector, could this have caused it not to be recognized by cubeprogrammer?

I had a F2 with 1.188 volt wich I could program, communicate with via programmercube

Now my stomahc is aching and I AM WEAK IN THE KNEES. Almost feel like passing out.

This one I couldnt program yet, but will check a few things.

Its 216 BGA on a custom board, I can see that I'm aligned judging from the vcaps, since 2 tiny islands underneat are at 1.125 and the bga is well flattened.

I have VDDA connected obviously.

Bypass reg grounded directly

PDR on VCC directly.

VDDDSI physically connected to VCAPDSI because I dont use.

BOOT0, BOOT1 pulled down

NRST pulled up and connected to debugger mini cortex header.

What else?

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
bassetteporn11
Associate II

hello? please tap my back?

bassetteporn11
Associate II

Well good thing I kept @ it.

It worked.

After messing up the first chip somehow and getting zero volt on vcap and having my soul pulled out.

I managed to grab the strenght to solder up a new chip, only to fail @ connecting the connector properly due to ****** pcb pads and then looking for an hour, and soldered all around the plastic making the support ******. And call it a day.

To then, manage to connect the header crooked due to all the ****** plastic, to then cry and be consoled by my girlfriend.

To then, wonder if maybe... And see. ROFL it was crooked, wich should be almost impossible.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.