2020-06-24 1:17 AM
Hello all, I just bought a ST-LINK-V3 set.
Also, I have checked the signal on vcc pin, but there are no voltage on vcc.
Is it correct?
Solved! Go to Solution.
2020-06-24 1:32 AM
These are denoted by T_VCC, not VCC (on CN4 apparently a misprint), these pins are used to *detect* the target voltage and set the thresholds for the buffers inside the ST-Link. See footnotes below the respective table for the connector in question in UM2448.
2020-06-24 1:32 AM
These are denoted by T_VCC, not VCC (on CN4 apparently a misprint), these pins are used to *detect* the target voltage and set the thresholds for the buffers inside the ST-Link. See footnotes below the respective table for the connector in question in UM2448.
2020-06-24 2:23 AM
Oh!~
Thank you Andreas,
I have see the description.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.