2020-09-11 6:23 AM
When connecting to my new STLNK-V3 I was asked to update the firmware. During firmware update I got an error message saying that the firmware update failed. Now the STLink is not recognized by the PC any more. Is there a way to flash the whole firmware e.g. using another STLink and a firmware file?
******************* GDI DUMP => Date : Fri Sep 11 14:36:54 2020
No ST-Link device detected.
Please connect it and then retry.
**** End of GDI DUMP ****
2020-09-11 6:38 AM
Did you try to un-and replug?
2020-09-11 6:50 AM
2020-09-11 7:04 AM
There are binaries of the V3 bootloade out there.
2020-09-12 1:22 AM
Thank you for your reply.
Fount them. The STLink is now recognized as USB device again, But it seems that there is also configuration data located at 0x080100000 missing. The upgrader tells me that it does not know how to upgrade the device. I think I have spend enough time on this. I will put the STLink into the electronic scrap bin.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.