2021-08-13 3:54 AM
ST-LINK V2 Programmer NOT working for STM32G0B1KET6N
Kindly help me to upload the program
Here i attached the schematic for your reference.
Solved! Go to Solution.
2021-08-13 4:31 AM
Hello @Sn.17
Try using latest release of STM32cubeProgrammer tool.
Check all connectors, USB cables and USB ports.
Make sure that your board is worked properly, maybe you can check with other boards.
I'm waiting for your update.
Please mark my answer as best by clicking on the "Select as Best" button if it fully solved your issue. This will help other users find this solution more quickly.
Imen
2021-08-13 4:31 AM
Hello @Sn.17
Try using latest release of STM32cubeProgrammer tool.
Check all connectors, USB cables and USB ports.
Make sure that your board is worked properly, maybe you can check with other boards.
I'm waiting for your update.
Please mark my answer as best by clicking on the "Select as Best" button if it fully solved your issue. This will help other users find this solution more quickly.
Imen
2021-08-13 6:09 AM
ST-LINK Utilities? That won't work with the G0 series
Watch also SWD clock rate, the CM0(+) parts won't clock at higher speeds.
Don't see a schematic, but unlikely to be the issue
2021-08-14 4:53 AM
I'm using a STM32G0B1CCU6, so not exactly the same as you. However I can program my device via Serial Wire.
My ST-LINK V2 have firmware V2J36S7 and I'm using STM32CubeProgrammer v2.5.0 on a Linux PC.
Command: <path>/STM32_Programmer.sh -c port=SWD mode=UR -q -d build/<applicationname>.bin 0x8000000 -v -g
PS. SWD freq is 4000 KHz, I haven't touched it.
//Michael
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.